Home Automation & Buildings
It is difficult for people living in an area with frequent earthquakes not to feel at least some anxiety. Our quake-absorbing "seismic isolator" technology is used in many homes to help ease these fears.
Quake-absorbing buildings

To protect life and property from earthquakes
There are two main types of anti-earthquake technology: "Quake resistance", which refers to strengthened columns, and using beams and walls designed to be resistant against quakes, and "seismic isolation" which are structures installed in foundations to absorb vibrations from the ground. If a building is directly connected to its foundations, it is also directly vulnerable to seismic vibrations. Seismic isolation structures are like a buffer that provides protection for the building. Illustrated are THK's quake-absorbing seismic isolation devices that use crossed LM Guides to greatly reduce the amount of vibration transmitted from the ground to the building above.
Products used
LM Guide (Linear Motion Guide)
The LM Guide (Linear Motion Guide) is our main product, which incorporates a component with a linear rolling motion into practical use for the first time in the world.
Ball Screw
The Ball Screw is a high-efficiency feed screw with the ball making a rolling motion between the screw axis and the nut.